Press release

Siemens Healthineers presents mammography system with groundbreaking new imaging technology

Published on September 28, 2023
<p><em>Not for publication in the USA</em></p><ul><li><strong>Mammomat B.brilliant delivers high-quality 3D images in just five seconds&nbsp;</strong></li><li><strong>Unique combination of speed with high depth resolution and area resolution&nbsp;</strong></li><li><strong>Fast acquisition time makes scan more comfortable for patients&nbsp;</strong></li></ul><p>At the annual congress of the European Society of Breast Imaging, September 28 to 30, 2023 in Valencia, Spain, Siemens Healthineers presents Mammomat B.brilliant<sup>1</sup>, a new mammography system with wide-angle tomosynthesis. In tomosynsthesis, the tube moves around the breast at a wide 50° angle, which is the largest angle available on the market. Together with a scan time of around five seconds, this is the fastest wide-angle tomosynthesis on the market – creating a 3D image with high depth resolution in the shortest time possible. In this way, abnormalities and microcalcifications in the tissue can be identified with a high level of accuracy. The acquisition speed is about 35% faster compared to other devices, making the examination more comfortable for patients. "Our systems have to provide meaningful answers in the shortest possible time. This is especially important in mammography, when the stressful uncertainty for patients must be reduced to a minimum. Only Mammomat B.brilliant offers this unique combination of speed, resolution and wide angle," says Verena Schön, Head of X-Ray Products at Siemens Healthineers.&nbsp;</p><p>"We are already benefiting from the significant benefits that Mammomat B.brilliant offers in our clinical routines. The speed of tomosynthesis is very impressive and the image quality is excellent. Together with the quick and convenient positioning of the patients, it is an excellent tool for us in mammography," says Dr. Machteld Keupers, UZ Leuven, Belgium.&nbsp;</p><p>Patient information and work steps are clearly visible from every angle on a prominent display monitor. The new ComfortMove function relieves users of physical strain, ensuring that physicians can easily and quickly adapt the device to the patient's anatomy. ComfortMove, the display and a positioning laser help to significantly accelerate scan preparation.&nbsp;</p><p>Mammomat B.brilliant is the first device from Siemens Healthineers with PlatinumTomo: the combination of wide-angle tomosynthesis, the new detector, the completely newly developed Flying Focus Spot tube and the Premia AI reconstruction to improve image quality. Flying focal spot technology is used for the first time in mammography: It prevents blurring effects caused by tube movements during tomosynthesis. This results in sharp images even at very high scanning speeds. In tomosynthesis, the X-ray tube moves in a circle around the breast, unlike conventional mammography, where it remains static – creating a three-dimensional image.</p>
1

Siemens Healthineers 2023

Siemens Healthineers AG (listed in Frankfurt, Germany: SHL) pioneers breakthroughs in healthcare. For everyone. Everywhere. As a leading medical technology company headquartered in Erlangen, Germany, Siemens Healthineers and its regional companies are continuously developing their product and service portfolio, with AI-supported applications and digital offerings that play an increasingly important role in the next generation of medical technology. These new applications will enhance the company’s foundation in in-vitro diagnostics, image-guided therapy, in-vivo diagnostics, and innovative cancer care. Siemens Healthineers also provides a range of services and solutions to enhance healthcare providers’ ability to provide high-quality, efficient care. In fiscal 2022, which ended on September 30, 2022, Siemens Healthineers, which has approximately 69,500 employees worldwide, generated revenue of around €21.7 billion and adjusted EBIT of almost €3.7 billion. Further information is available at www.siemens-healthineers.com.