Proprietary Strip Technology Allows for Proper Results Reporting

Siemens proprietary strip technology (Auto-Checks) on the CLINITEK Status+ Analyzer demonstrates better results reporting for humidity-exposed urine test strips.

In an article published in the column “Tips from the Clinical Expert” in the online version of Medical Laboratory Observer (September 2011) entitled “Evaluation of an automated humidity check for instrument-read urinalysis strips”, 3 different brands of urine test strips were tested for their ability to detect humidity exposure which could compromise strip integrity and lead to false results. Of the 3 urine test strips tested, Siemens’ Multistix® 10 SG reagent strip on the CLINITEK Status®+ analyzer was the only system capable of detecting over-exposure to humidity. Using its proprietary Auto-Checks technology, the CLINITEK Status analyzer has the capability to generate a printed error message and will not report potentially erroneous results in these situations.

The strips evaluated were:

  • CHEMSTRIP 10 MD (Roche Diagnostics)
  • Multistix 10 SG (Siemens)
  • Clarity UROCHECK 10SG (Diagnostic Test Group)

According to the results, “the Siemens system has an automatic warning mechanism that prevents results from being reported when humidity exposure is detected. In this controlled study, approximately 98% of the time, this system would have prevented inaccurate reporting and generated an error message instead of generating a result.”

Read the following article on the MLO web site:

“Evaluation of an automated humidity check for instrument-read urinalysis strips”

 

For more information on these products:

The Multistix 10 SG reagent strip is the reliable, frontline test for the detection of a broad range of conditions, from detecting urinary tract infections (UTI) to diabetes and kidney disorders.

The CLINITEK Status+ Analyzer features new automatic quality checks (Auto-Checks) providing improved clinical information.

The products/features shown on this webpage are not commercially available in all countries. Due to regulatory reasons their future availability cannot be guaranteed. Please contact your local Siemens organization for further details.