Evaluation of Single Vessel Coronary Artery Disease with IQ•SPECT

Guillaume Bouchard, MD, Hopital Cite-de-la-Sante, Laval, Quebec, Canada |  2013-12-01

History

An asymptomatic 80-year-old female (61 kg/134 lbs) with previously diagnosed mild Coronary Artery Disease (CAD) presented with complaints of exertional dyspnea. The patient had an angiography in 1998, which showed 50% stenosis of the left main coronary artery for which the patient preferred medical therapy and non-invasive follow-up. The last myocardial perfusion imaging (MPI) pharmacologic stress study in May 2010 was normal (not shown). The patient underwent Technetium sestamibi (99mTc MIBI) myocardial perfusion SPECT in January 2012 using IQ•SPECT performed on a Symbia™ T2 SPECT•CT system.

Evaluation

An IQ•SPECT MPI performed using dipyridamole stress and rest in January 2012, showed new severe and extensive, but reversible perfusion defect in the inferolateral and inferobasal wall (proximal right coronary artery territory). There was no significant poststress left ventricle (LV) dilatation (normal TID). Resting left ventricle ejection fraction (LVEF) was normal and showed normal response to stress. There were no significant EKG changes during the dipyridamole stress test. In view of the severe reversible ischemia in the right coronary artery (RCA) territory in a patient with known 50% left main coronary artery stenosis, a coronary angiogram was ordered.

A coronary angiography revealed 40-50% distal left main stenosis, which reflects stable CAD since 1998. There was a new and severe, 95% proximal right coronary subocclusion, exactly as suspected by MPI, which was the culprit lesion. Excellent restoration of RCA flow with no residual stenosis was obtained after angioplasty. The patient presented subsequently with atypical and mostly epigastric pain and underwent a follow-up MPI study using IQ•SPECT with the same protocol in January 2013, which showed complete resolution of ischemia.

Examination Protocol

Scanner         Symbia T2 SPECT•CT

Scan Dose     25 mCi 99mTc sestamibi

Parameters    17 Frames 9 sec/frame

CT                 Low-dose CT for attenuation correction

Comments

This case example clearly defines the value of stress rest myocardial perfusion scintigraphy in detecting inducible ischemia, guiding the subsequent decision for coronary angiography and stenting of proximal RCA stenosis. A follow-up perfusion study also defined complete resolution of ischemia with normalization of perfusion pattern, which correlated well with resolution of clinical symptoms. With fast cardiac MPI acquisitions of just 4 minutes using IQ•SPECT, there is further improvement in patients’ tolerance levels for myocardial perfusion studies. This is particularly so in elderly patients, as shown in this case.

The statements by Siemens Healthineers' customers described herein are based on results that were achieved in the customer's unique setting. Since there is no "typical" hospital and many variables exist (e.g., hospital size, case mix, level of IT adoption) there can be no guarantee that other customers will achieve the same results.