Head/Neck 64

Ultra-fast, high SNR, head and neck imaging

Head/Neck 64
 
Get a Quote

Hear what customers and collaboration partners say

"The 64-Channel Head/Neck coil allows us to get better signals from the cortex and also cover the cerebellum and the neck very well. That allows exploration of new research fields which are difficult to do with other coils."1

Prof. Rainer Goebel, PhD (MAGNETOM Prismafit user)
Professor, Maastricht University & Scientific Director,
Scannexus, Maastricht, The Netherlands

"The Head/Neck 64 reveals previously hard-to-recognize, but pertinent anatomical and disease-related details for a spectrum of pathologies within the brain, inner ear, orbits, skull base and neck, as well as the cervical spinal cord. This leads to improved insight into neuro-anatomy relevant to an extended range of diseases. All this can be achieved, fortunately, at advanced speed and resolution."1
Prof. Dr. med. Bernhard Schuknecht, MD
Diagnostic, Vascular and Interventional Neuroradiology
MRI-Medical Radiological Institutes Zurich, Switzerland
 

“I think that at the end of the day, we produced a very high quality coil and it will be usable with almost any patient and it has succeeded in extending the coverage of the 32 channel brain array down into the spine.”1

Lawrence Wald, PhD
Director, MGH NMR Core, Martinos Center
MGH, Boston, USA

"And this has relevance, for example, for neurodegenerative diseases, for multiple sclerosis, where the spinal cord is heavily involved. Or for pain studies or motor learning or functional plasticity of the central nervous system."1
Boris Keil, PhD
Assistant in Biomedical Engineering
MGH, Boston, USA

"Collaboration was great [...] I think the success of the enterprise, the fact that this prototype worked first time out, really spoke, not just to the brilliance of Boris and Larry and the design, but to the closeness of the interactions that we had with our colleagues at Siemens to provide us all the key information and hardware we needed to design and build a successful coil."1
Bruce Rosen, PhD
Director Athinoula A. Martinos Center for Biomedical Imaging
MGH, Boston, USA

 


Clinical Images

Large FoV, ultra-fast, head and neck imaging with high iPAT factors

High-resolution C-spine imaging

Non contrast-enhanced ToF imaging of the brain and carotids

High-resolution whole-brain DTI Tractography

High-resolution C-spine Tractography with RESOLVE

Download the Head/Neck 64 flyer for more examples and clinical cases.

General Requirements

System

Minimum Software Version

syngo MR D13A
syngo MR D13D

Other

Also available for:

MAGNETOM Prismafit

MAGNETOM Skyrafit

64-Channel configuration

Scanner upgrade may be necessary

 

Please Note: Additional technical pre-requisites may apply. Upon receiving your request, your local Siemens representative will clarify whether your system meets the requirements.

Related Products, Services & Resources

The products/features shown on this webpage are not commercially available in all countries. Due to regulatory reasons their future availability cannot be guaranteed. Please contact your local Siemens Healthineers organization for further details.

1The statements by Siemens Healthineers' customers described herein are based on results that were achieved in the customer's unique setting. Since there is no "typical" hospital and many variables exist (e.g., hospital size, case mix, level of IT adoption) there can be no guarantee that other customers will achieve the same results.