ZOOMit powered by TimTX TrueShape

ZOOMit powered by TimTX TrueShape
 
Try

With ZOOMit you can zoom into the anatomy and shape your image according to the region of interest. This enables the highlighting
of regions, organs, or features of an organ.

Overall benefits of the the parallel transmit application ZOOMit

  • Increase in diagnostics confidence
  • Open up new MR imaging fields
  • Expand research possibilities
  • And, now with TimTX Acceleration2 ZOOMit is brought to a new level, providing 20% higher SNR1

 


Clinical Benefits: See more details. In less time.

ZOOMit is currently enabled for DWI, BOLD and T2 SPACE 3D imaging. 3D imaging like MSK, spine or brain profits the most from the ZOOMit induced scan time reduction. Diffusion based imaging profits from the significantly increased image quality.

High resolution 3D imaging, with shorter acquisition times.

ZOOMit can dramatically reduce scan time.In this comparison between conventional and zoomed imaging, scan time is reduced by 45% while maintaining the same high resolution.

High-quality diffusion-weighted imaging

Quality of DWI is especially crucial when this technique is used for the
detection of smallest lesions of high susceptibility (e.g.skull base, spine, abdomen, pelvis), or when quantification of diffusion restriction is required.

ZOOMit gives exactly that:
Significantly increased image quality in the area of interest. In this example of an MR diffusion in the prostate, the zoomed images have much less distortion and better delineation of tumor borders.

“The conventional DWI sequence in the Head & Neck is very challenging. With TimTX TrueShape, we achieve the same spatial resolution but with shorter echo trains – so we have less distortions.”3

Professor Henrik Michaely, MD
University Medical Center Mannheim, Germany
Dr. Philipp Riffel, MD,
University Medical Center, Mannheim, Germany


Technical Details:

It is a well-known phenomenon in MR imaging that if the field-of-view (FOV) is smaller than the object, aliasing (foldover artifacts) will occur. This is not an issue in the readout direction, since it can be overcome by frequency oversampling. But oversampling in the phase-encoding direction comes at a cost: longer scan times. This makes the use of phase oversampling unfavorable or impossible in many cases.

With ZOOMit, similar to an optical zoom of a camera, only a reduced FOV in phase-encoding direction (‘stripe’) is excited (see figure below). Consequently, there will be no signal from the non-excited regions and only the small stripe needs to be encoded.
The result: Acquisition time can be reduced while maintaining spatial resolution, or the spatial resolution can be increased - or a combination thereof.


Hardware and Software Requirement: TimTX TrueShape

ZOOMit is based on TimTX TrueShape, Siemens’ architecture for parallel transmit (pTX) technology. This technology uses two indepedent transmit channels for fully dynamic RF excitation. Only TimTX TrueShape and ZOOMit together provide selective excitation within a user specified FoV. TimTX TrueShape is designed to break ground for a broad range of new MRI applications. ZOOMit is the first TrueShape application.
For further information: www.siemens.com/TrueShape

General Requirements

System

Minimum Software Version

syngo MR D13C

syngo MR D13D

Other

TimTX TrueShape
Please Note: Additional technical pre-requisites may apply. Upon receiving your request, your local Siemens representative will clarify whether your system meets the requirements.

Related Products, Services & Resources

1Results may vary. Data on file.

2Available only with syngo MR E11A. The product may not be commercially available in all countries. Due to regulatory reasons its future availability cannot be guaranteed. Please contact your local Siemens organization for further details.

3The statements by Siemens Healthineers' customers described herein are based on results that were achieved in the customer's unique setting. Since there is no "typical" hospital and many variables exist (e.g., hospital size, case mix, level of IT adoption) there can be no guarantee that other customers will achieve the same results.