RESOLVE: A Powerful Tool for Imaging the Pediatric Spine

Laura L. Hayes, M.D.; et al.
Department of Radiology, Children’s Healthcare of Atlanta at Scottish Rite, Atlanta, GA, USA
 |  Mar 14, 2014

Until recently, clinically useful diffusion-weighted imaging (DWI) of the spine has not been possible using standard single shot EPI techniques due to susceptibility artifacts and the need for higher spatial resolution. The novel 2D-navigator-corrected readout-segmented EPI sequence known as RESOLVE can obtain images with higher spatial resolution and reduced distortion of the spine related to susceptibility, pulsations, respiration and motion.

This is especially helpful when imaging children where the small size of their spine/cord, prominent CSF and arterial pulsations, and higher pulse and respiratory rates compared to adults can pose significant limitations on the quality of the images obtained. Motion artifacts that notoriously plague every facet of pediatric imaging are also reduced with RESOLVE.


Protocols

Related Articles

The information presented is for illustration only and is not intended to be relied upon by the reader for instruction as to the practice of medicine. Any health care practitioner reading this information is reminded that they must use their own learning, training and expertise in dealing with their individual patients. This material does not substitute for that duty and is not intended by Siemens Healthineers to be used for any purpose in that regard.

The drugs and doses mentioned herein are consistent with the approval labelling for uses and/or indications of the drug. The treating physician bears the sole responsibility for the diagnosis and treatment of patients, including drugs and doses prescribed in connection with such use. The Operating Instructions must always be strictly followed when operating the system. The source for the technical data is the corresponding data sheets. Results may vary.