Case Report: Knee MR Imaging of an Osteochondroma in Combination with Melorheostosis

Paul Flechsig, M.D.; Marc-André Weber, M.D.
University Hospital Heidelberg, Heidelberg, Germany
 |  2011-12-18

In daily patient care imaging speed and high resolution are key elements that are in direct conflict.
In this issue Professor Marc-André Weber et al. (University Hospital Heidelberg, Germany) present a case of cartilaginous exostosis (osteochondroma) that shows how combining 3T MRI and dedicated high-density coils provides an irreplaceable tool for the fast and accurate evaluation of malignant and benign aspects and helps to raise arguments against a parosteal osteosarcoma or a low-grade chondrosarcoma as differential diagnoses.


The information presented is for illustration only and is not intended to be relied upon by the reader for instruction as to the practice of medicine. Any health care practitioner reading this information is reminded that they must use their own learning, training and expertise in dealing with their individual patients. This material does not substitute for that duty and is not intended by Siemens Healthineers to be used for any purpose in that regard.

The drugs and doses mentioned herein are consistent with the approval labelling for uses and/or indications of the drug. The treating physician bears the sole responsibility for the diagnosis and treatment of patients, including drugs and doses prescribed in connection with such use. The Operating Instructions must always be strictly followed when operating the system. The source for the technical data is the corresponding data sheets. Results may vary.