Knee MR Imaging of Haemarthrosis in a Case of Haemophilia A

Marc-André Weber, M.D., et al.
University Hospital Heidelberg, Germany
 |  2010-07-20

Imaging pediatric joints is often still a domain of x-ray and ultrasound. However, the application of MRI is of growing importance not only because of excellent soft tissue contrast and its superior capacity to visualize and evaluate the extension of involvement of soft tissues but also because of its capability to early and precisely detect bone destruction. In this case, Prof. Marc-André Weber, University of Heidelberg, Germany, reports on the imaging findings of a 14-year-old male with known haemophilia A.


Further Reading

The information presented is for illustration only and is not intended to be relied upon by the reader for instruction as to the practice of medicine. Any health care practitioner reading this information is reminded that they must use their own learning, training and expertise in dealing with their individual patients. This material does not substitute for that duty and is not intended by Siemens Healthineers to be used for any purpose in that regard.

The drugs and doses mentioned herein are consistent with the approval labelling for uses and/or indications of the drug. The treating physician bears the sole responsibility for the diagnosis and treatment of patients, including drugs and doses prescribed in connection with such use. The Operating Instructions must always be strictly followed when operating the system. The source for the technical data is the corresponding data sheets. Results may vary.