Motion management comes of age

3min
Published on October 23, 2017

Motion management is crucial if you want to achieve high resolution in PET/CT. Respiratory gating solutions compensate for respiratory motion and help to increase image quality.

It’s quite possible that the most common sentence uttered by PET/CT technicians is “now lie still.” Getting the patient to be still is important for producing clear images. But even the most obedient patients must continue to breathe, and their hearts must continue to beat. There is motion in the human body that simply can’t be avoided.

“Motion management is mandatory if you want to achieve high resolution,” says Frank M. Bengel, MD, Director of the Department of Nuclear Medicine at the Klinik fur Nuklearmedizin, Medizinische Hochschule Hannover, in Germany. “You need to compensate for the motion because the motion-derived blurring of the cardiovascular structures will abolish any benefit that you would have from high resolution. You also need to correct for respiratory motion. If you can do that […] then we can get great images of any cardiovascular structure, maybe not just chamber walls but also smaller structures like valves.” Motion must be compensated for since it cannot be eliminated.


Download your print version here.

Siemens Healthineers’ respiratory motion management tools provide respiratory gating solutions that help improve delineation and quantification of small lesions. These motion management tools integrate the control of the respiratory monitoring device into the scanner user interface, thereby helping to accelerate the workflow. This integration also allows operators to view the respiratory curve directly on the acquisition console for a quick visual quality control.

Additionally, CardioFreeze, a new cardiac motion management feature that employs dual-gating technology, aides in the examination of the human heart. CardioFreeze divides images into multiple gates and then reconstructs them to provide physicians information on cardiovascular performance.

Static images show multiple hypermetabolic liver metastases, some of which appear elongated with respiratory-motion-related blurring

Figure 1: Static images show multiple hypermetabolic liver metastases, some of which appear elongated with respiratory-motion-related blurring. OncoFreeze images show similar sharp delineation of the liver metastases, but with high overall image quality and count statistics and low noise levels along with high lesion-to-background ratio.1

“[Motion Management gives you] a series of images that, if you play them in sequence, show you the way the heart beats and contracts. It reduces the respiratory motion so you get a truer image of how the heart is functioning,” says Sebastian Fuerst, PhD, a senior systems engineer at Siemens Healthineers. He compares the system to photographing something that is in rapid motion. “Think of photographing a tennis ball after it has been hit. If the shot exposure is too long, then the image will be blurry. If you open the shutter for a very short amount of time, then you might be able to clearly see the tennis ball. What motion management does is efficiently manage the amount of exposure.


Fuerst explains that respiratory gating provides better information to doctors and clinicians. “You can examine a respiratory wave more precisely, deciding which parts you are most interested in. You can take advantage of [a lot of] additional data that you have acquired.” While the motion management feature is robust, there are still challenges for clinicians.

Respiratory gates are able to provide clear images.

Figure 2: PET/CT myocardial viability study at rest shows a large infarct involving most of inferior wall and apex with thinned out but viable myocardium in the septum. Dilated left ventricular cavity with a low ejection fraction of 26% at rest suggests severe ventricular dysfunction.2

“There is no such thing [as an image free of noise],” Fuerst states. “We’ve been pushing the sensitivity of PET scanners over the years to detect as much of the activity injected into the patient as possible. It all boils down to lesion detectability. With respiratory motion, we can see a sort of blurring [in the images], making the lesions appear large and making the boundaries unclear. Our new technology provides physicians with all the data that is acquired in a scan and by that, [we are] improving/reducing the noise levels of the images.”