Discovering Pantai Kelanang, A Coastal Gem Just an Hour from Kuala Lumpur4 November 2023

As part of our World Environment Campaign, 30 volunteers from Siemens Healthineers Malaysia teamed up once again with local NGO MY Clean Beach to address environmental challenges at “Pantai Kelanang” (Kelanang Beach), a hidden gem within the coastal area just an hour's drive from Kuala Lumpur. It's hard to believe that this beautiful beach is located on the outskirts of the city, nestled within a community filled with greenery.

Pantai Kelanang, Mohrib

|2023-11-04

The area we focused on was located slightly away, requiring a 15-minute trek from the main beach. This beach location, dubbed “off Kelanang Beach," bears sights of local fish and a beautiful sandy beach often used for picnics and wedding photo shoots

However, what we saw was a dose of reality: the local environment facing threats from washed-up waste, plastics clad and tarpaulins deeply entrenched in the sand, and the usual litter that marries the beauty of this pristine coastline!

Undeterred by the sight (and the obvious challenge), our dedicated volunteers, over the next 90 minutes, diligently collected, sorted, and loaded about 447.5 kilograms of trash onto the waiting truck.

Here is the raw breakdown of what we hauled in:

  • General Waste: 85 kg
  • Plastic: 138.8 kg
  • Glass: 20.2 kg
  • Tin/Metal: 3.5 kg
  • Large items: 200 kg
This experience has prompted us to reflect on the importance of building a culture of change. It goes beyond just saving the planet; it is about instigating a shift in mindset and fostering teamwork. The 447.5 kilograms of trash collected is not just a statistic; it represents our collective effort to make a positive impact on the environment we all share.

We owe our gratitude to My Clean Beach for suggesting Off Pantai Kelanang for our community service efforts. While well-known beaches often receive the spotlight, there are countless lesser-visited gems along the coast that deserve attention, especially those off the main beach areas that hide beautiful local fauna.

As we celebrate this mini outcome, we acknowledge that this is merely the beginning. No grand promises, just a genuine push for more eco-friendly initiatives. We aim to be part of the solution, working towards a sustainable future. 🌱💙

Special thanks to our video partner, Nusantara Visual, who actively participated in the clean-up and documented the entire activity. Check out the video they produced, capturing the essence of our commitment to a cleaner, healthier planet!

#MalaysiaWeCan