Photon-counting Detectors in Clinical Computed Tomography

Stefan Ulzheimer, Steffen Kappler |  Jan 12, 2017

The detector system is arguably the key component in a computed tomography scanner. Its task is to convert the incoming X-rays into an electrical signal that can then be fed into the image reconstruction chain. Decisive properties are high quantum efficiency (X-ray stopping power), large dynamic range, and fast signal decay (low afterglow) combined with excellent signal stability.


CT detectors – permanently enhanced

CT detectors have undergone many development steps from the very early gas detectors – sometimes radical, sometimes merely incremental. Based on its proprietary scintillator material UFCTM, Siemens continuously sets new standards in CT detector design.[1] The latest innovation is the fully integrated StellarInfinity detector that Siemens uses in today’s high-end CT systems (Fig. 1), first introduced with SOMATOM Force. Due to its unprecedented level of electronic integration, the StellarInfinity detector delivers exceptionally low levels of electronic noise and high signal dynamics. This makes it the optimal tool to exploit current and future iterative reconstruction possibilities.

Fig. 1: First-generation detectors still used Xenon gas under high pressure to convert the incoming X-rays into electric current. Second-generation detectors use solid-state ceramic scintillators to convert X-rays into light, photodiodes to convert light into current, and analog-to-digital converters (ADC) to digitize the signal. The Stellar detector is the first third-generation detector that combines the photodiode and the ADC in one application-specific integrated circuit (ASIC), dramatically reducing electronic noise, power consumption, and heat dissipation. Photon-counting detectors1 have the potential to revolutionize CT imaging.


Today’s solid-state detectors use a two-step process to convert the incoming X-ray intensity into an electronic signal. First, the X-rays are converted into visible light in a scintillator layer. Below, the figure shows a photodiode array that converts the emitted light into an electric current that is digitized in dedicated ASICs. The scintillator layer is made of a ceramic material that is mechanically structured into pixels. Septa of finite width separate the individual pixels in order to suppress optical cross-talk (Fig. 2A).

The next step: photon-counting detectors1

Semiconductor materials such as cadmium telluride (CdTe) are able to convert X-rays directly into electric signal pulses. Each incoming X-ray quantum generates clouds of free charge carriers with the amount of free charges being proportional to the energy of the incident X-ray beam. A strong electrical field inside the detector material transports the charge clouds to anode pixels (Fig. 2B) in which an electrical current is induced. Highly integrated circuits transform these charge pulses into voltage pulses of a few nanoseconds duration that can be counted digitally.

So far, CdTe has not been used in commercially available clinical CT scanner detectors for the following reasons:

  • The goal of photon-counting detectors is to register each X-ray individually. Due to the large diameter of the scanned patient in a clinical setting, a relatively large number of X-ray beams is required to reach the detector in a very short time. In clinical whole body CT imaging – even with the low dose levels used today – the time between two X-rays that arrive at an individual pixel can be as short as a couple of nanoseconds. Therefore, the detector electronics have to be extremely fast and precise.
  • Signal stability in CT scans is of the utmost importance. Even the slightest stability variations in the detector signal can lead to visible ring artifacts in the CT images. Production of crystalline materials with the purity and excellent signal stability required to achieve diagnostic image quality in a whole body CT scanner has not yet been possible.

Multi-energy information

If such detectors, however, do become available, they will offer tremendous advantages. It would not only be possible to register or count each individual photon but also to measure the energy from each individual photon. Without any other technical prerequisites, multi-energy CT could become possible. In principle, as a next step following on from dual energy CT, an arbitrary number of energies is achievable. Still, in order to limit the amount of data delivered by the detector, it is more practical to put the registered photons within certain energy ranges or “energy bins” and only read the data for these bins. Today’s dual energy CT is sufficient for the materials present in the human body and for iodine contrast. More “bins” would not add more information here. Should new contrast materials become available in the future, however, such as gold nanoparticles with additional absorption peaks in the used X-ray energy range,[2] three, four, or even more, bins might be beneficial (k-edge imaging).

Lower dose and higher spatial resolution

Since only signal pulses above a certain threshold are registered in photon-counting CT scanning, such detectors completely eliminate electronic noise that is produced in every electronic component until a signal is digitized. The StellarInfinity detector set a new standard with exceptionally low electronic noise due to its complete integration of photodiodes and analog-digital convertors in one single chip. There are clear advantages in clinical scenarios of using extremely low doses [3] or when having to deal with low signals such as in obese patients. Photon-counting detectors will take this to a new level. In addition, photon-counting detectors are able to weigh low-energy photons higher than high-energy photons. This allows even further optimization of the contrast-to-noise ratio (CNR) in contrast-enhanced applications. Initial studies show that an additional dose reduction of 32% will be possible.[4]

In today’s scintillators, the pixels have to be mechanically structured and therefore cannot be infinitely small. With decreasing pixel size, the geometrical dose efficiency drops because the relative area of the septa between the pixels increases. In photon-counting detectors, a mechanical separation of the pixels is not necessary. Pixels can be structured in a photolithographic process as already established for silicon chips. In principle, pixels can be made very small. Of course, an optimized value must also be found here that delivers practical additional clinical value. Recent publications in the field of computed tomography indicate that the pixel pitch in photon-counting detectors for clinical scanners might be reduced by a factor of three to four relative to today’s solid-state detectors.

Prototype installations

Siemens is the first medical equipment company to be able to demonstrate the potential of high-flux capable photon-counting technology in two near-clinical prototype installations.[5,6] The prototypes are based on SOMATOM Definition Flash hardware in which the second detector system was replaced with a photon-counting detector. For the first time, clinical equivalence comparable to existing technology was demonstrated in human subjects. In the next five years, Siemens will collaborate with its network of partners to optimize the technology and to identify new clinical potentials.


About the Author

Stefan Ulzheimer, PhD, Siemens Healthineers, Germany
Steffen Kappler, PhD, Siemens Healthineers, Germany


Share this page:

[1] Ulzheimer S, “Stellar Detector Performance in Computed Tomography”. SOMATOM Sessions. 2011 Nov; 29:64-66.

[2] Cormode DP, Naha PC, Fayad ZA. Nanoparticle contrast agents for computed tomography: a focus on micelles. Contrast Media Mol Imaging. 2014 Jan-Feb;9(1):37-52.

[3] Ebner L, Knobloch F, Huber A, Landau J, Ott D, Heverhagen JT, Christe A. Feasible Dose Reduction in Routine Chest Computed Tomography Maintaining Constant Image Quality Using the Last Three Scanner Generations: From Filtered Back Projection to Sinogram-affirmed Iterative Reconstruction and Impact of the Novel Fully Integrated Detector Design Minimizing Electronic Noise. J Clin Imaging Sci. 2014 Jul 31;4:38.

[4] S. Kappler et al., First results from a hybrid prototype CT scanner for exploring benefits of quantum-counting in clinical CT, Proc. SPIE 8313, pp. 83130X (2012).

[5] Zhicong Yu, Shuai Leng, Steven M Jorgensen, Zhoubo Li, Ralf Gutjahr, Baiyu Chen, Ahmed F Halaweish, Steffen Kappler, Lifeng Yu, Erik L Ritman and Cynthia H McCollough. Evaluation of conventional imaging performance in a research whole-body CT system with a photon-counting detector array. Phys. Med. Biol. 61 (2016) 1572–1595

[6] Pourmorteza A, Symons R, Sandfort V, Mallek M, Fuld MK, Henderson G, Jones EC, Malayeri AA, Folio LR, Bluemke DA. Abdominal Imaging with Contrast-enhanced Photon-counting CT: First Human Experience. Radiology. 2016 Feb 3:152601.

1The product is still under development and not commercially available yet. Its future availability cannot be guaranteed.