Switch off the Auto Trigger function when using Bolus Tracking

ago 05, 2009

It is possible to switch off this function. You can use the advantage of monitoring the contrast enhancement during the injection and start the scan when desired manually. On the following screenshot you will see where you can switch the Auto Trigger off. Also on the Trigger Subtask you get a message that the Auto Trigger function is disabled.