Did you know that it is possible to save an image directly in a JPEG-format in syngo InSpace?

Dec 10, 2008

For example, when you create an image and want to use it in a presentation, you do a right mouse click on the "Save As" icon (indicated in red on the image), and select the desired format. Alternately, if you are using a USB-device that is supported by our software, you can save the image directly to it.