How to speed up workflow

Nov 01, 2010

The newest versions of syngo CT 2010A, syngo CT 2010B and syngo MMWP 2009B now include InSpace 4D. One important advantage of this new feature is that while loading a dataset, the table removal calculation can be done automatically in the background, resulting in a faster workflow, increased productivity and less mouse clicks.

You can activate this feature as follows:
Open syngo InSpace 4D.
Select “InSpace” and then “Settings” in the menu bar. (Marked in red on the image). Place the markers on the same positions as in the example. (Marked in green on the image).
From now on, every time a dataset is loaded, calculation of the table removal will be done automatically in the background.