Getting to the heart of it with syngo.via1!

май 01, 2011

It is often easier to evaluate the heart valves with various image settings. As is shown on the image, the cusps of the aortic valve are better differentiated. To do this, please use the invert option within syngo.via* (Marked in red on the image). Get access to this option via the right lower corner menu.

1syngo.via can be used as a stand-alone device or together with a variety of syngo.via-based software options which are medical devices on their own rights.