Favorite scan protocol at the top

Dec 01, 2010

The scan protocol which is used the most can easily be placed at the top of all the scan protocols, for an easy and fast access.

For this example the “AbdomenRoutine” scan protocol is used the most and the user wants to change the position in the list. (See image 1)
In the Scan Protocol Assistant it is possible the place a scan protocol where ever you want.

How to start:
1. Open the Scan Protocol Assistant and select the entry “Manipulate scan protocols (cut/copy/paste/delete)”.
2. In Step 2 select a scan protocol with the left mouse button and drag it to the desired position.
(See image 2)
3. Confirm the changes in Step 3.
From now on the scan protocol will be stored on the preferred position. (See image 3)