Easily edit the centerline in InSpace AVA

Jan 01, 2009

During analysis of the vessels in syngo InSpace 4D AVA (Advanced Vessel Analysis), you can easily edit or delete points on the centerline. Select the "Edit" function (marked in green on image 1) then select the Vessel mode (marked in red on image 1). In the cross-sectional MPR, MPR or VRT, you can select the green handles and then drag them to the desired place or delete them with the delete button on your keyboard. The centerline will then be updated automatically (image 2).