Dual Energy Abdominal CTA

SOMATOM Definition abdominal CTA with direct dual energy bone subtraction

Alec J Megibow M.D., M.P.H, F.A.C.R; Johnny Vlahos, M.D.
Department of Radiology, NYU Medical Center, New York, USA
 |  фев 27, 2007

History

A 75-year-old man was referred for pre-surgical MDCT evaluation of a known abdominal aortic aneurysm that had been detected on screening abdominal ultrasound. A contrast enhanced CTA scan of the abdomen was performed on the SOMATOM Definition.


Diagnosis
The acquisition parameters allowed precise localization of the origin of the aneurysm with respect to the renal arteries and allowed for necessary measurements of the neck of the aneurysm, the distance from the renal arteries to the aortic bifurcation and to each common iliac bifurcation to be calculated, and the adequacy of the run-off to the lower extremities to be assessed. Finally, a small accessory renal artery supplying the upper pole of the right kidney was detected. Based on this single study, the patient was considered a candidate for endovascular repair.

 

Comments
The scanning protocol (outlined below) utilized the Definition’s dual x-ray sources each operating at a different kVp thereby resulting in a simultaneous dual energy acquisition. Two spiral data sets are acquired in a single acquisition; each data set contains unique spectral information, which allows differentiation and characterization of imaged structures and tissue (Figure 1). In this Dual Energy application, the direct subtraction of bone can be achieved almost instantly with a high degree of accuracy as compared with conventional bone removal techniques. Additionally, critical small vessels such as an accessory right upper pole renal artery can be easily preserved. Using Dual Energy acquisitions, abdominal CTA segmentations can be performed eliminating manual post processing steps thereby significantly reducing reporting time. The degree of bone segmentation is at the discretion of the radiologist; in this example, the dual display allows the vascular map to be superimposed over the skeletal structures. This aids the surgeon in establishing landmarks that can aid in the fluoroscopic based endovascular repair. The success of the bone removal is illustrated in the MIP image (Figure 2).
 

Fig. 1: Precise visualization of the abdominal aneurysm and their relations to skeletal landmarks is possible with SOMATOM Definition.
Fig. 2: Dual Energy MIP of the abdominal vasculature allows to immediate rule out aneurysms, stenosis or embolism. Notice the lack of interference from bones.
Fig. 3: Dual Energy VRT, excellent visualization of the abdominal skeleton.
 

Examination Protocol

 

Scanner SOMATOM Definition
Scan area Abdominal Angiography
Scan length 410 mm
Scan time 12 sec
Scan direction Caudo-cranial
kV 140 kV and 80 kV
Effective mAs 66 eff. mAs and 190 eff. mAs
Rotation time 0.5 sec
Slice collimation 0.6 mm
Spatial resolution 0.33 mm
Slice width 2 mm
Reconstructed slice thickness 2 mm
Increment 1.5 mm
CTDIvol 10.7 mGy
Kernel D20f
Contrast material volume 100 ml
Flow rate 4 ml/s
Bolus tracking On

 

The information presented is for illustration only and is not intended to be relied upon by the reader for instruction as to the practice of medicine. Any health care practitioner reading this information is reminded that they must use their own learning, training and expertise in dealing with their individual patients. This material does not substitute for that duty and is not intended by Siemens Healthineers to be used for any purpose in that regard.

The drugs and doses mentioned herein are consistent with the approval labelling for uses and/or indications of the drug. The treating physician bears the sole responsibility for the diagnosis and treatment of patients, including drugs and doses prescribed in connection with such use. The Operating Instructions must always be strictly followed when operating the system. The source for the technical data is the corresponding data sheets. Results may vary.